Hello,
yes, the DCSS may be used for scaling:
use section 7 (Multimedia) of "i.MX_Linux_Release_Notes.pdf" and section 6.3.5 [Display
Control Subsystem (DCSS)] of ''i.MX_Reference_Manual.pdf".
https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.