IMX6Q-SABREAUTO EVK board boot failed using Android 9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q-SABREAUTO EVK board boot failed using Android 9

1,486件の閲覧回数
mayqueen
Contributor IV

Platform: IMX6Q

OS: Android 9 (p9.0.0-2.2.0-ga)

As title, I tried the android 9 on IMX6Q-SABREAUTO EVK board but boot failed, it looks good before running into system, but it shows services failed when start running  zygote..

log:

type=1400 audit(1562322318.470:10255): avc: denied { dac_read_search } for pid=1072 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0
type=1400 audit(1562322319.730:10256): avc: denied { dac_read_search } for pid=241 comm="Binder:241_4" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0
init: Received control message 'interface_start' for '[email protected]::ISensors/default' from pid: 190 (/system/bin/hwservicemanager)
init: Could not find service hosting interface [email protected]::ISensors/default
init: Received control message 'interface_start' for '[email protected]::ISensors/default' from pid: 190 (/system/bin/hwservicemanager)
init: Could not find service hosting interface [email protected]::ISensors/default
healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a

Seems the sensors service has some problem, but it also shows the same messages when I take out the sensors configuration from device/fsl/imx6dq/sabreauto_6q/sabreauto_6q.mk

Any directions? I stocking almost one week... thanks

タグ(2)
0 件の賞賛
返信
1 返信

1,367件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello May,

   For i.MX6Q, use android 8.0 BSP, please!   Android 9.0 does't support i.MX6Q.

Hope above information can help you.

Have a nice day!
BR,

Weidong

0 件の賞賛
返信