i.MX8M SW Video Encoder Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M SW Video Encoder Linux

Jump to solution
7,566 Views
choppad
Contributor II

Hello i.MX Community Gurus?

The i.MX8M does not have a Hardware based H.264 Video Encoder, rather the documentation says that the NXP i.MX8M uses a Software based H.264 Video Encoder.  I have been unsuccessful in finding this software encoder.  Will someone please provide this software encoder such that it can be leveraged throughout the i.MX8M community? pastedImage_1.png

Thanks in Advance,

DeWayne

Tags (2)
0 Kudos
Reply
1 Solution
6,413 Views
choppad
Contributor II

Hello:

I have found the following SW Video Encoder solution that "should work" on i.MX8M, but not too sure.  Will someone from the community please advise?

x264, the best H.264/AVC encoder - VideoLAN 

x264 is a free software library and application for encoding video streams into theH.264/MPEG-4 AVC compression format, and is released under the terms of the GNU GPL.

I'm hoping that this helps!

DeWayne 

View solution in original post

0 Kudos
Reply
6 Replies
6,414 Views
choppad
Contributor II

Hello:

I have found the following SW Video Encoder solution that "should work" on i.MX8M, but not too sure.  Will someone from the community please advise?

x264, the best H.264/AVC encoder - VideoLAN 

x264 is a free software library and application for encoding video streams into theH.264/MPEG-4 AVC compression format, and is released under the terms of the GNU GPL.

I'm hoping that this helps!

DeWayne 

0 Kudos
Reply
6,413 Views
joanxie
NXP TechSupport
NXP TechSupport

you also can try to use build the gst-libav, then use the encoder there.

 

0 Kudos
Reply
6,413 Views
choppad
Contributor II

Hello Joan:

I appreciate your response.  Will you please advise the steps to build gst-libav, and then subsequently how to "use the encoder there"?

0 Kudos
Reply
6,413 Views
joanxie
NXP TechSupport
NXP TechSupport

one can refer to the linux user guide,. which tell you how to install gstreamer1.0-libav into rootfs, for the SW encoder, maybe the performance isn't good enough, customer needs to improve it by yourself.

0 Kudos
Reply
6,413 Views
choppad
Contributor II

Joan:

I appreciate your response, however, the CODECs that are inclusive in that download are Audio CODECs.  What I am inquiring about is the H.264 SW Video Encoder.  

Please Advise,

DeWayne

0 Kudos
Reply
6,413 Views
joanxie
NXP TechSupport
NXP TechSupport

the yocto should contain these codec, if you need AACP, you can download from the link as below, pls focus on the "

Codecs and other Algorithms (2)":

i.MX 8M Evaluation Kit|NXP 


for more detailed information about codec in the bsp, pls refer to the i.MX Linux® Release Notes

0 Kudos
Reply