i.MX8M-Plus CSI1 maximum resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8M-Plus CSI1 maximum resolution

1,226 次查看
malik_cisse
Senior Contributor I

Hi there,

There are 2 CSI interfaces on the imx8mp: CSI0 and CSI1.

As you can see in the picture attached, the second imx8mp CSI interface (CSI1) runs with a 266Mhz pixel clock.

Does this have limitations in terms of maximum image resolution? So is it possible to transmit 4K@30fps images (3840x2160) on this CSI1?

The usage scenario: Use either CSI0 or CSI1 (only one at a time and stop the unused interface).

BR, MC

0 项奖励
回复
0 回复数