Hi all,
we meeting a very serious problem on i.mx8mm,
tested with BSP:4.14.98_2.3.0 & 4.19.35_1.1.0)。
when pilot run over 250pcs customization board,
but almost have 4% board meet the issues
system maybe freeze sometime when run memtester for burn in
or complete memtest cycle
the issues like cpufreq scaling driver not stable?
have anyone give me some advise for debug?
the board design to reference i.mx8mm EVK
run DDR stress tool passed over night
[ 6764.162531] rcu: rcu_sched kthread starved for 5252 jiffies! g100017 f0x0 RCU_GP_WAIT_FQS(5) ->state=0x402 ->cpu=2
[ 6764.172875] rcu: RCU grace-period kthread stack dump:
[ 6764.177924] rcu_sched I 0 11 2 0x00000028
[ 6764.183410] Call trace:
[ 6764.185856] __switch_to+0xdc/0x148
[ 6764.189345] __schedule+0x1d8/0x5c8
[ 6764.192833] schedule+0x38/0xa0
[ 6764.195975] schedule_timeout+0x90/0x368
[ 6764.199900] rcu_gp_kthread+0x494/0x860
[ 6764.203737] kthread+0x128/0x130
[ 6764.206965] ret_from_fork+0x10/0x18
[ 6827.030347] rcu: INFO: rcu_sched detected stalls on CPUs/tasks:
[ 6827.036286] rcu: 2-...!: (0 ticks this GP) idle=c50/0/0x0 softirq=109760/109760 fqs=1
[ 6827.044287] rcu: (detected by 3, t=21007 jiffies, g=100017, q=7)
[ 6827.050383] Task dump for CPU 2:
[ 6827.053610] swapper/2 R running task 0 0 1 0x00000028
[ 6827.060660] Call trace:
[ 6827.063114] __switch_to+0xdc/0x148
[ 6827.066603] 0xffff800035158000
[ 6827.069747] rcu: rcu_sched kthread starved for 15755 jiffies! g100017 f0x0 RCU_GP_WAIT_FQS(5) ->state=0x402 ->cpu=2
[ 6827.080178] rcu: RCU grace-period kthread stack dump:
[ 6827.085227] rcu_sched I 0 11 2 0x00000028
[ 6827.090713] Call trace:
[ 6827.093159] __switch_to+0xdc/0x148
[ 6827.096650] __schedule+0x1d8/0x5c8
[ 6827.100138] schedule+0x38/0xa0
[ 6827.103281] schedule_timeout+0x90/0x368
[ 6827.107206] rcu_gp_kthread+0x494/0x860
[ 6827.111042] kthread+0x128/0x130
[ 6827.114271] ret_from_fork+0x10/0x18
[ 7137.266393] cpu cpu0: failed to scale arm_reg down: -110
[ 7137.271773] cpufreq: __target_index: Failed to change cpu frequency: -110
[ 7137.694380] cpu cpu0: failed to scale arm_reg down: -110
[ 7137.699751] cpufreq: __target_index: Failed to change cpu frequency: -110
[ 7138.122540] cpu cpu0: failed to scale arm_reg down: -110
[ 7138.128097] cpufreq: __target_index: Failed to change cpu frequency: -110
[ 7138.550539] cpu cpu0: failed to scale arm_reg down: -110
[ 7138.556091] cpufreq: __target_index: Failed to change cpu frequency: -110
Hi kunyichen
one can try attached patch, however it is highly recommended to use
latest bsps, described on linux documentation link
additionally one can try to change signals drive strength (search in RPA tool for "stregth").
Best regards
igor