Hi.
I am trying to run secure hello-world example on imx8m-mini without success.
My board is from variscite running Linux kernel 4.14.78. I followed instruction to compile tee-supplicant and hello-world host and secure examples.
Running tee-supplicant gives me the error:
./tee-supplicant
ERR [11475] TSUP:main:694: failed to find an OP-TEE supplicant device
In my kernel configuration I have:
CONFIG_TEE=y
# TEE drivers
CONFIG_OPTEE=y
And in Device tree I added:
firmware {
optee {
compatible = "linaro,optee-tz";
method = "smc";
};
};
When system boots I see no /dev/tee in /dev folder and dmesg output is:
optee: probing for conduit method from DT.
optee: api uid mismatch
I tried changing "smc" to "hvc" in device tree method, but the result is the same.
How can I fix this so I can run the code hello-world examples?
Sorry for posting again, but I'm not able to edit my previous post anymore (time expired!?).
BTW: According to NXPs "i.MX Porting Guide", the device tree node for optee on i.MX8 processors is added dynamically by u-boot, so you're not meant to patch the devicetree manually.
Hello,
just in case anyone else has this problem and finds this thread, this worked for me with Variscite VAR-SOM-MX8M-MINI, Yocto Warrior 2.7 and kernel 4.19.35:
I added " optee" by a MACHINE_FEATURES_append statement in “local.conf”. (Don't make the same mistake as me and put it in a recipe, as this will probably result in “imx-atf” and “imx-boot” builds without optee support, due to delayed statement evaluation.)
DISTRO_FEATURES of the fsl distro should contain "optee" by default, so "optee" ends up in COMBINED_FEATURES and all modifications for this feature are applied.
After modprobing the kernel module, xtest runs without problems.
Best regards
djoh
Hello,
Unfortunately, we cannot provide support for the Variscite BSP. Since is a different one that we currently support for our Boards. I suggest you is to submit a ticket with Variscite.
Variscite Support Center - Variscite
I apologize for the inconveniences this could give you.
Best regards,
Diego.