i.MX8M Mini SAI3 UART2 RTS/CTS configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini SAI3 UART2 RTS/CTS configuration

1,696 Views
john_weber
Contributor II

It seems that the SAI3 UART2 configuration is missing from the pins-imx8mm.h file in the dt-bindings. Can you please take a look at the attached patch and confirm that it should work?

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,601 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

We do not have ported the UART since the pin is already ported in the SAI3_RXC for the UART2_CTS and the SAI3_RXD for the UART2_RTS. These pins are already in use.

I apologize for the inconveniences that this could give.

Best regards,

Diego.

0 Kudos
Reply