Using DMA in imx6ul SPI client driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using DMA in imx6ul SPI client driver

2,640 Views
uuwen
Contributor I

According to this link, it seems that DMA support can be enabled by setting "dma-names" in dts. Also referring to this thread and checking it, the DMA related driver code is also integrated in spi-imx.c.

I am writing a driver for a SPI SRAM device and am using the 23k256 driver (/drivers/mtd/devices/mchp23k256.c) as reference. It seems to me that the IMX SPI controller driver is already handling the DMA mappings and requests, and there is no extra configuration needed other than calling standard SPI API as illustrated in the 23k256 driver?

Labels (4)
1 Reply

2,349 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chin

you are right, there is no extra configuration needed other than calling standard SPI APIs.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------