i.MX8M Mini SAI3 UART2 RTS/CTS configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini SAI3 UART2 RTS/CTS configuration

1,681件の閲覧回数
john_weber
Contributor II

It seems that the SAI3 UART2 configuration is missing from the pins-imx8mm.h file in the dt-bindings. Can you please take a look at the attached patch and confirm that it should work?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,586件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

We do not have ported the UART since the pin is already ported in the SAI3_RXC for the UART2_CTS and the SAI3_RXD for the UART2_RTS. These pins are already in use.

I apologize for the inconveniences that this could give.

Best regards,

Diego.

0 件の賞賛
返信