i.MX8M Mini L2 cache access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini L2 cache access

ソリューションへジャンプ
1,986件の閲覧回数
m_c
Senior Contributor I

Is it possible to acess L2 cache in bare metal mode (jailhouse inmate)? If not, which memory has fastest access time that bare matel mode can access?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,848件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

seems not as discussed on arm forum:

Using the whole Cortex-A L2 Cache without external memory - Cortex-A / A-Profile forum - Processors ... 

DDR memory would be fastest access as it is designed for such purpose.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,849件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

seems not as discussed on arm forum:

Using the whole Cortex-A L2 Cache without external memory - Cortex-A / A-Profile forum - Processors ... 

DDR memory would be fastest access as it is designed for such purpose.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信