i.MX8M GPU test oom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M GPU test oom

Jump to solution
3,998 Views
m_c
Senior Contributor I

Customer try to running "/unit_tests/GPU/gpu.sh" repeatedly on i.MX8M and found out of memory after a while. Also found the free memory is getting lower.

1. Is there any memory leak in gpu unit test?

2. Increase kernel parameter cma will solve it?

Labels (1)
0 Kudos
Reply
1 Solution
3,915 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

I sent additional details regarding this issue via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,800 Views
CordialMai
Contributor I

Hello m_c:

Have you sloved this issue?

Can you tell me how to slove it,I met a similar issue.

Thank you very much!

Best reguards!

CordialMai

0 Kudos
Reply
3,916 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

I sent additional details regarding this issue via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply