i.MX8M GPU test oom

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,004件の閲覧回数
m_c
Senior Contributor I

Customer try to running "/unit_tests/GPU/gpu.sh" repeatedly on i.MX8M and found out of memory after a while. Also found the free memory is getting lower.

1. Is there any memory leak in gpu unit test?

2. Increase kernel parameter cma will solve it?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,921件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

I sent additional details regarding this issue via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,806件の閲覧回数
CordialMai
Contributor I

Hello m_c:

Have you sloved this issue?

Can you tell me how to slove it,I met a similar issue.

Thank you very much!

Best reguards!

CordialMai

0 件の賞賛
返信
3,922件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

I sent additional details regarding this issue via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信