i.MX8M DRAM Controller Data width

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M DRAM Controller Data width

ソリューションへジャンプ
1,563件の閲覧回数
dixit_jz
Contributor I

Hi,

I have learned from the datasheet of i.MX8M that the data width supported by the DRAM controller of the processor is only x16 and x32. Whereas, I can understand from the pinout that there are four pairs of data strobes and four data masks available. Can I make use of these signals to connect four numbers of  x8 memory ICs.

Or are these only meant for Quad die, Dual channel package devices like the one used in the EVK.

Regards,

Dixit

ラベル(1)
0 件の賞賛
返信
1 解決策
1,490件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dixit

>Can I make use of these signals to connect four numbers of  x8 memory ICs

yes this is possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,491件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dixit

>Can I make use of these signals to connect four numbers of  x8 memory ICs

yes this is possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信