i.MX8DualX+ Power Up Timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8DualX+ Power Up Timing

1,946件の閲覧回数
jbrayadec
Contributor I

Hello,

Section 4.2.1 "Power-up Sequence" lists the order in which the i.MX8Quad/DualX power supplies need to come up for proper operation.  It says that each power group can power up in sequence or "simultaneously" with the other groups.  How close to hitting their nominal voltage do they need to be to be considered "simultaneous"?

Thanks,

Jeff

0 件の賞賛
返信
3 返答(返信)

1,930件の閲覧回数
jbrayadec
Contributor I

Thanks for the reply, but maybe my question wasn't clear enough.  I'm looking for the timing of the power supplies coming up to their nominal voltages as listed in Table 9.  For example, if they all come up and are stable with 1us of each other is that suitable?  What about 5us?  10us?  

Thanks,

Jeff

0 件の賞賛
返信

1,927件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

if they are stable with 0us of each other (immediately) it is suitable.

 

Best regards
igor

0 件の賞賛
返信

1,935件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jbrayadec

 

regarding "How close to hitting their nominal voltage", voltage should be within

range specified Table 9. Operating ranges

i.MX 8DualX Industrial Applications Processors - Data Sheet

Also sect.4.2.1 has Note:

 

The definition of “power-up” refers to a stable voltage operating within the
range defined in Table 9.

 

Best regards
igor

0 件の賞賛
返信