i.MX8 support RCCC camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 support RCCC camera

1,928 Views
xu_ji1
Contributor V

Hi,

Does i.MX8 support RCCC  RAW output 12bit camera?how to config the ISI driver about 

 mxc_isi_out_formats[]

Thanks

0 Kudos
Reply
3 Replies

1,876 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

it is supported by hardware but nxp linux bsp does not support

such configuration. Currently supported formats can be found in driver

mxc-isi-cap.c\imx8\platform\media\drivers - linux-imx - i.MX Linux kernel 

For porting and testing camera driver may be useful unit test

mx8_v4l2_cap_drm.c\mxc_v4l2_test\test - imx-test - i.MX Driver Test Application Software 

also may be helpful:

MX8 CSI - Variscite Wiki 

GStreamer Based Image Signal Processor - IMX8 Pipelines 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,876 Views
xu_ji1
Contributor V

Hi,

How to make BSP support it?

0 Kudos
Reply

1,876 Views
igorpadykov
NXP Employee
NXP Employee

>How to make BSP support it?

you can make porting yourself or apply for help to

Commercial Support and Engineering Services | NXP 

Best regards
igor

0 Kudos
Reply