i.MX8 Camera CSI MIPI question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8 Camera CSI MIPI question

Jump to solution
1,572 Views
xu_ji1
Contributor V

Hello,

If we want to changed MIPI_CSI_CLK N and P/MIPI_CSI_DATA N and P each other,

like use MIPI_CSI_CLK_N as MIPI_CSI_CLK_P / MIPI_CSI_DATA_N as MIPI_CSI_DATA_P,whereas.

Does it support this on i.MX8 platform?Is there some method to changed in SW side?

Thanks

0 Kudos
Reply
1 Solution
1,481 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

unfortunately such change is not supported in hardware nor software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,482 Views
igorpadykov
NXP Employee
NXP Employee

Hi Xu

unfortunately such change is not supported in hardware nor software.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply