i.MX7DRM About CS1 on Port A of QuadSPI configuration parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7DRM About CS1 on Port A of QuadSPI configuration parameters

Jump to solution
1,526 Views
minoru_nishimura
Contributor II

Hello,

I have a question about CS1 on Port A.
When I set the serial flash port B selection to 0, are the following settings correct?

1 – Enable CS1 on Port A
0 – Disable CS1 on Port B


Regards,

Nomu

Labels (1)
0 Kudos
Reply
1 Solution
1,519 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

yes this setting is correct.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
5 Replies
1,520 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

yes this setting is correct.

 

Best regards
igor

0 Kudos
Reply
1,488 Views
minoru_nishimura
Contributor II

Hi Igor

 

I have an additional question,
Will Serial flash A2 stop working with the following settings?

0 – Port B is not used.

0 – Disable CS1 on Port A

0 – Disable CS1 on Port B

 

Best regards

Nomu

0 Kudos
Reply
1,483 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

with "Disable CS1 on Port A" setting only CS0 port A will continue to work.

 

1.jpg

 

Best regards
igor

1,466 Views
minoru_nishimura
Contributor II

Hi Igor

I have an additional question,
Is CS0 port A the same as QSPIn_A_SS0_B?


Best regards

Nomu

0 Kudos
Reply
1,463 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

>Is CS0 port A the same as QSPIn_A_SS0_B?

yes


Best regards
igor