i.MX7DRM About CS1 on Port A of QuadSPI configuration parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7DRM About CS1 on Port A of QuadSPI configuration parameters

ソリューションへジャンプ
2,396件の閲覧回数
minoru_nishimura
Contributor II

Hello,

I have a question about CS1 on Port A.
When I set the serial flash port B selection to 0, are the following settings correct?

1 – Enable CS1 on Port A
0 – Disable CS1 on Port B


Regards,

Nomu

ラベル(1)
0 件の賞賛
返信
1 解決策
2,389件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

yes this setting is correct.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,390件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

yes this setting is correct.

 

Best regards
igor

0 件の賞賛
返信
2,358件の閲覧回数
minoru_nishimura
Contributor II

Hi Igor

 

I have an additional question,
Will Serial flash A2 stop working with the following settings?

0 – Port B is not used.

0 – Disable CS1 on Port A

0 – Disable CS1 on Port B

 

Best regards

Nomu

0 件の賞賛
返信
2,353件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

with "Disable CS1 on Port A" setting only CS0 port A will continue to work.

 

1.jpg

 

Best regards
igor

2,336件の閲覧回数
minoru_nishimura
Contributor II

Hi Igor

I have an additional question,
Is CS0 port A the same as QSPIn_A_SS0_B?


Best regards

Nomu

0 件の賞賛
返信
2,333件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

>Is CS0 port A the same as QSPIn_A_SS0_B?

yes


Best regards
igor