i.MX7DRM About CS1 on Port A of QuadSPI configuration parameters

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX7DRM About CS1 on Port A of QuadSPI configuration parameters

跳至解决方案
2,295 次查看
minoru_nishimura
Contributor II

Hello,

I have a question about CS1 on Port A.
When I set the serial flash port B selection to 0, are the following settings correct?

1 – Enable CS1 on Port A
0 – Disable CS1 on Port B


Regards,

Nomu

标签 (1)
0 项奖励
回复
1 解答
2,288 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

yes this setting is correct.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,289 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

yes this setting is correct.

 

Best regards
igor

0 项奖励
回复
2,257 次查看
minoru_nishimura
Contributor II

Hi Igor

 

I have an additional question,
Will Serial flash A2 stop working with the following settings?

0 – Port B is not used.

0 – Disable CS1 on Port A

0 – Disable CS1 on Port B

 

Best regards

Nomu

0 项奖励
回复
2,252 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

with "Disable CS1 on Port A" setting only CS0 port A will continue to work.

 

1.jpg

 

Best regards
igor

2,235 次查看
minoru_nishimura
Contributor II

Hi Igor

I have an additional question,
Is CS0 port A the same as QSPIn_A_SS0_B?


Best regards

Nomu

0 项奖励
回复
2,232 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nomu

 

>Is CS0 port A the same as QSPIn_A_SS0_B?

yes


Best regards
igor