Hello,
I have a question about CS1 on Port A.
When I set the serial flash port B selection to 0, are the following settings correct?
1 – Enable CS1 on Port A
0 – Disable CS1 on Port B
Regards,
Nomu
Solved! Go to Solution.
Hi Nomu
yes this setting is correct.
Best regards
igor
Hi Igor
I have an additional question,
Will Serial flash A2 stop working with the following settings?
0 – Port B is not used.
0 – Disable CS1 on Port A
0 – Disable CS1 on Port B
Best regards
Nomu
Hi Nomu
with "Disable CS1 on Port A" setting only CS0 port A will continue to work.
Best regards
igor
Hi Igor
I have an additional question,
Is CS0 port A the same as QSPIn_A_SS0_B?
Best regards
Nomu
Hi Nomu
>Is CS0 port A the same as QSPIn_A_SS0_B?
yes
Best regards
igor