i.MX7D clock source and power up sequence issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX7D clock source and power up sequence issue

2,126 次查看
felixhsu
Contributor III

Hi All

The customer use i.MX7D platform have two issue,

1. the clock source will start before  VDD_SNVS_IN, this situation have any concern?

2. the i.MX7D with PMIC PF3000, when first time power up have twice trigger PMIC_ON_REQ and NVCC_SD1, this situation is normal or not? how to explanation this phenomenon?

As below is scope measurement result.

scope.png

Thanks.

标签 (5)
0 项奖励
回复
5 回复数

1,948 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Felix

>1. the clock source will start before  VDD_SNVS_IN, this situation have any concern?

no external voltages/signals should be applied to processor before completion power-up sequence.

>2. the i.MX7D with PMIC PF3000, when first time power up have twice trigger PMIC_ON_REQ

>and NVCC_SD1, this situation is normal or not?

please check power-up sequence and sect.2. i.MX7DS design checklist

Hardware Development Guide for i.MX7Dual and 7Solo Applications Processors
http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,948 次查看
felixhsu
Contributor III

Hi Igor

1. so external clock should be same time with  VDD_SNVS_IN, right?

2. the Hardware Development Guide which part have explanation twice trigger PMIC_ON_REQ and NVCC_SD1?

Thanks

0 项奖励
回复

1,948 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Felix

>1. so external clock should be same time with  VDD_SNVS_IN, right?

no.

No external voltages/signals should be applied to processor before completion power-up sequence.

Best regards
igor

0 项奖励
回复

1,948 次查看
felixhsu
Contributor III

Hi Igor

About question 2, do you have any comments?

I can not found related explanation in the document.

Thanks.

0 项奖励
回复

1,948 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Felix

for question 2 unfortunately I am not aware of documents describing in details.

Suggest follow Hardware Guide.

Best regards
igor

0 项奖励
回复