i.MX7D clock source and power up sequence issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7D clock source and power up sequence issue

2,090件の閲覧回数
felixhsu
Contributor III

Hi All

The customer use i.MX7D platform have two issue,

1. the clock source will start before  VDD_SNVS_IN, this situation have any concern?

2. the i.MX7D with PMIC PF3000, when first time power up have twice trigger PMIC_ON_REQ and NVCC_SD1, this situation is normal or not? how to explanation this phenomenon?

As below is scope measurement result.

scope.png

Thanks.

ラベル(5)
0 件の賞賛
返信
5 返答(返信)

1,912件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

>1. the clock source will start before  VDD_SNVS_IN, this situation have any concern?

no external voltages/signals should be applied to processor before completion power-up sequence.

>2. the i.MX7D with PMIC PF3000, when first time power up have twice trigger PMIC_ON_REQ

>and NVCC_SD1, this situation is normal or not?

please check power-up sequence and sect.2. i.MX7DS design checklist

Hardware Development Guide for i.MX7Dual and 7Solo Applications Processors
http://www.nxp.com/files/32bit/doc/user_guide/IMX7DSHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,912件の閲覧回数
felixhsu
Contributor III

Hi Igor

1. so external clock should be same time with  VDD_SNVS_IN, right?

2. the Hardware Development Guide which part have explanation twice trigger PMIC_ON_REQ and NVCC_SD1?

Thanks

0 件の賞賛
返信

1,912件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

>1. so external clock should be same time with  VDD_SNVS_IN, right?

no.

No external voltages/signals should be applied to processor before completion power-up sequence.

Best regards
igor

0 件の賞賛
返信

1,912件の閲覧回数
felixhsu
Contributor III

Hi Igor

About question 2, do you have any comments?

I can not found related explanation in the document.

Thanks.

0 件の賞賛
返信

1,912件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Felix

for question 2 unfortunately I am not aware of documents describing in details.

Suggest follow Hardware Guide.

Best regards
igor

0 件の賞賛
返信