i.MX7 LPDDR2 byte and bit swapping.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7 LPDDR2 byte and bit swapping.

ソリューションへジャンプ
2,276件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX7 LPDDR2 layout.

They want to use byte swapping and bit swapping with LPDDR2, but there is no hardware design guide for i.MX7 to judge whether it is ok or not.

So would you give us advise whether they can use byte swapping and bit swapping or not for LPDDR2 with i.MX7?

Best Regards,

Satoshi Shimoda

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,999件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Strictly speaking, JEDEC provides pad sequence standardization for LPDDR2 :

"Ordering of DQ bits shall be maintained in the system, including within the

package and on the PCB. DQ byte swapping and DQ bit Swapping are not allowed in

the system."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,000件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Strictly speaking, JEDEC provides pad sequence standardization for LPDDR2 :

"Ordering of DQ bits shall be maintained in the system, including within the

package and on the PCB. DQ byte swapping and DQ bit Swapping are not allowed in

the system."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,999件の閲覧回数
satoshishimoda
Senior Contributor I

Hello Yuri,

Thank you for your quick response.

OK, I understood that byte and bit swapping are prohibited for LPDDR2.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信