i.MX7 Firmware development without YOCTO Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX7 Firmware development without YOCTO Project

1,603件の閲覧回数
axaykumarrana
Contributor I

Hello,

I would like to know that is there any way we can develop firmware for i.MX series processors to run specific algorithms?

Yocto project is great however it seems that I need to code kernals/drivers for my custom board based on i.MX7 which would be using peripherals for further processing.

Any hints are appreciated. 

タグ(3)
0 件の賞賛
返信
1 返信

1,478件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

 Hi  Axaykumar

one can check Eclipse usage and FreeRTOS
https://community.freescale.com/docs/DOC-103736
https://www.nxp.com/webapp/Download?colCode=FreeRTOS_iMX7D_1.0.1_LINUX&appType=license&Parent_nodeId...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信