i.MX7 Firmware development without YOCTO Project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX7 Firmware development without YOCTO Project

1,589 次查看
axaykumarrana
Contributor I

Hello,

I would like to know that is there any way we can develop firmware for i.MX series processors to run specific algorithms?

Yocto project is great however it seems that I need to code kernals/drivers for my custom board based on i.MX7 which would be using peripherals for further processing.

Any hints are appreciated. 

标记 (3)
0 项奖励
回复
1 回复

1,464 次查看
igorpadykov
NXP Employee
NXP Employee

 Hi  Axaykumar

one can check Eclipse usage and FreeRTOS
https://community.freescale.com/docs/DOC-103736
https://www.nxp.com/webapp/Download?colCode=FreeRTOS_iMX7D_1.0.1_LINUX&appType=license&Parent_nodeId...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复