Hello,
I am trying to interface with PLX switch ic and 4 FPGAs using PCIe.
During pcie bring up sequence, I got memory assign errors as follows.
How can I increase pcie mem space?
Kernel 3.0.35
| root@freescale ~$ lspci | |
| 00:00.0 Class 0604: 16c3:abcd | |
| 01:00.0 Class 0604: 10b5:8624 | |
| 02:01.0 Class 0604: 10b5:8624 | |
| 02:04.0 Class 0604: 10b5:8624 | |
| 02:05.0 Class 0604: 10b5:8624 | |
| 02:06.0 Class 0604: 10b5:8624 | |
| 02:08.0 Class 0604: 10b5:8624 | |
| 02:09.0 Class 0604: 10b5:8624 | |
| 05:00.0 Class 1180: 1b03:7800 |
06:00.0 Class 1180: 1b03:7800
I got follow dmesg
| root@freescale ~$ dmesg | grep pci | |
| iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering. | |
| PCIE: imx_pcie_pltfm_probe start link up. | |
| pci 0000:00:00.0: [16c3:abcd] type 1 class 0x000604 | |
| pci 0000:00:00.0: reg 10: [mem 0x00000000-0x000fffff 64bit pref] | |
| pci 0000:00:00.0: reg 38: [mem 0x00000000-0x0000ffff pref] | |
| pci 0000:00:00.0: supports D1 | |
| pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold | |
| pci 0000:00:00.0: PME# disabled | |
| pci 0000:01:00.0: [10b5:8624] type 1 class 0x000604 | |
| pci 0000:01:00.0: reg 10: [mem 0x00000000-0x0001ffff] | |
| pci 0000:01:00.0: PME# supported from D0 D3hot D3cold | |
| pci 0000:01:00.0: PME# disabled | |
| pci 0000:02:01.0: [10b5:8624] type 1 class 0x000604 | |
| pci 0000:02:01.0: PME# supported from D0 D3hot D3cold | |
| pci 0000:02:01.0: PME# disabled | |
| pci 0000:02:04.0: [10b5:8624] type 1 class 0x000604 | |
| pci 0000:02:04.0: PME# supported from D0 D3hot D3cold | |
| pci 0000:02:04.0: PME# disabled | |
| pci 0000:02:05.0: [10b5:8624] type 1 class 0x000604 | |
| pci 0000:02:05.0: PME# supported from D0 D3hot D3cold | |
| pci 0000:02:05.0: PME# disabled | |
| pci 0000:02:06.0: [10b5:8624] type 1 class 0x000604 | |
| pci 0000:02:06.0: PME# supported from D0 D3hot D3cold | |
| pci 0000:02:06.0: PME# disabled | |
| pci 0000:02:08.0: [10b5:8624] type 1 class 0x000604 | |
| pci 0000:02:08.0: PME# supported from D0 D3hot D3cold | |
| pci 0000:02:08.0: PME# disabled | |
| pci 0000:02:09.0: [10b5:8624] type 1 class 0x000604 | |
| pci 0000:02:09.0: PME# supported from D0 D3hot D3cold | |
| pci 0000:02:09.0: PME# disabled | |
| pci 0000:05:00.0: [1b03:7800] type 0 class 0x001180 | |
| pci 0000:05:00.0: reg 10: [mem 0x00000000-0x0003ffff] | |
| pci 0000:05:00.0: reg 14: [mem 0x00000000-0x007fffff] | |
| pci 0000:05:00.0: reg 18: [mem 0x00000000-0x007fffff] | |
| pci 0000:05:00.0: reg 1c: [mem 0x00000000-0x00ffffff] | |
| pci 0000:05:00.0: reg 20: [mem 0x00000000-0x01ffffff] | |
| pci 0000:06:00.0: [1b03:7800] type 0 class 0x001180 | |
| pci 0000:06:00.0: reg 10: [mem 0x00000000-0x0003ffff] | |
| pci 0000:06:00.0: reg 14: [mem 0x00000000-0x007fffff] | |
| pci 0000:06:00.0: reg 18: [mem 0x00000000-0x007fffff] | |
| pci 0000:06:00.0: reg 1c: [mem 0x00000000-0x00ffffff] | |
| pci 0000:06:00.0: reg 20: [mem 0x00000000-0x01ffffff] | |
| pci 0000:00:00.0: BAR 8: can't assign mem (size 0x8a00000) | |
| pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff 64bit pref] |
pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff 64bit pref] (PCI add)
| pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref] | |
| pci 0000:01:00.0: BAR 8: can't assign mem (size 0x8800000) | |
| pci 0000:01:00.0: BAR 0: can't assign mem (size 0x20000) | |
| pci 0000:02:05.0: BAR 8: can't assign mem (size 0x4400000) | |
| pci 0000:02:06.0: BAR 8: can't assign mem (size 0x4400000) | |
| pci 0000:02:01.0: PCI bridge to [bus 03-03] | |
| pci 0000:02:01.0: bridge window [io disabled] | |
| pci 0000:02:01.0: bridge window [mem disabled] | |
| pci 0000:02:01.0: bridge window [mem pref disabled] | |
| pci 0000:02:04.0: PCI bridge to [bus 04-04] | |
| pci 0000:02:04.0: bridge window [io disabled] | |
| pci 0000:02:04.0: bridge window [mem disabled] | |
| pci 0000:02:04.0: bridge window [mem pref disabled] | |
| pci 0000:05:00.0: BAR 4: can't assign mem (size 0x2000000) | |
| pci 0000:05:00.0: BAR 3: can't assign mem (size 0x1000000) | |
| pci 0000:05:00.0: BAR 1: can't assign mem (size 0x800000) | |
| pci 0000:05:00.0: BAR 2: can't assign mem (size 0x800000) | |
| pci 0000:05:00.0: BAR 0: can't assign mem (size 0x40000) | |
| pci 0000:02:05.0: PCI bridge to [bus 05-05] | |
| pci 0000:02:05.0: bridge window [io disabled] | |
| pci 0000:02:05.0: bridge window [mem disabled] | |
| pci 0000:02:05.0: bridge window [mem pref disabled] | |
| pci 0000:06:00.0: BAR 4: can't assign mem (size 0x2000000) | |
| pci 0000:06:00.0: BAR 3: can't assign mem (size 0x1000000) | |
| pci 0000:06:00.0: BAR 1: can't assign mem (size 0x800000) | |
| pci 0000:06:00.0: BAR 2: can't assign mem (size 0x800000) | |
| pci 0000:06:00.0: BAR 0: can't assign mem (size 0x40000) | |
| pci 0000:02:06.0: PCI bridge to [bus 06-06] | |
| pci 0000:02:06.0: bridge window [io disabled] | |
| pci 0000:02:06.0: bridge window [mem disabled] | |
| pci 0000:02:06.0: bridge window [mem pref disabled] | |
| pci 0000:02:08.0: PCI bridge to [bus 07-07] | |
| pci 0000:02:08.0: bridge window [io disabled] | |
| pci 0000:02:08.0: bridge window [mem disabled] | |
| pci 0000:02:08.0: bridge window [mem pref disabled] | |
| pci 0000:02:09.0: PCI bridge to [bus 08-08] | |
| pci 0000:02:09.0: bridge window [io disabled] | |
| pci 0000:02:09.0: bridge window [mem disabled] | |
| pci 0000:02:09.0: bridge window [mem pref disabled] | |
| pci 0000:01:00.0: PCI bridge to [bus 02-08] | |
| pci 0000:01:00.0: bridge window [io disabled] | |
| pci 0000:01:00.0: bridge window [mem disabled] | |
| pci 0000:01:00.0: bridge window [mem pref disabled] | |
| pci 0000:00:00.0: PCI bridge to [bus 01-08] | |
| pci 0000:00:00.0: bridge window [io disabled] | |
| pci 0000:00:00.0: bridge window [mem disabled] |
pci 0000:00:00.0: bridge window [mem pref disabled]
Best regards
Hi,
We tried to modify the kernel source to increase PCIE Memory regions as follows
PCIE_ARB_BASE_ADDR and PCIE_ARB_END_ADDR in mx6.h.
/* CPU Memory Map */
#define PCIE_ARB_BASE_ADDR 0xE0000000
#define PCIE_ARB_END_ADDR 0xFFFFFFFF
But System crash happened in function imx_pcie_regions_setup.
I am curious about the fundamental question whether it is possible to increase
PCIe memory by modifying or not? moreover, Can we assign memory resource to another place?
Best regards
Aden Yoon
Hello,
Please try the recent BSP L.3.14.28
In particular You may look at section 42.3 (System Resource: Memory Layout) of
“i.MX_6_Linux_Reference_Manual.pdf” regarding PCIe memory usage.
Total memory size is up to 16 MB.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
I have similar issue where my device driver failed to allocate memory for the bars and I am using 3.14.28
imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [io 0x1000-0x10000]
pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]
pci_bus 0000:00: root bus resource [bus 00-ff]
pci_bus 0000:00: scanning bus
pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400
pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]
pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref]
pci 0000:00:00.0: calling pci_fixup_ide_bases+0x0/0x3c
pci 0000:00:00.0: supports D1
pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
pci 0000:00:00.0: PME# disabled
pci_bus 0000:00: fixups for bus
PCI: bus0: Fast back to back transfers disabled
pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0
pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1
pci_bus 0000:01: scanning bus
pci 0000:01:00.0: [1a33:8201] type 00 class 0x040000
pci 0000:01:00.0: reg 0x10: [mem 0xff000000-0xffffffff]
pci 0000:01:00.0: reg 0x20: [mem 0xffff0000-0xffffffff]
pci 0000:01:00.0: reg 0x24: [mem 0xfffff000-0xffffffff]
pci 0000:01:00.0: calling pci_fixup_ide_bases+0x0/0x3c
pci 0000:01:00.0: PME# supported from D0 D3hot
pci 0000:01:00.0: PME# disabled
pci_bus 0000:01: fixups for bus
PCI: bus1: Fast back to back transfers disabled
pci_bus 0000:01: bus scan returning with max=01
pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
pci_bus 0000:00: bus scan returning with max=01
pci 0000:00:00.0: fixup irq: got 20
pci 0000:00:00.0: assigning IRQ 20
pci 0000:01:00.0: fixup irq: got 20
pci 0000:01:00.0: assigning IRQ 20
pci 0000:00:00.0: BAR 14: can't assign mem (size 0x1800000)
pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]
pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff] (PCI address [0x1000000-0x10fffff])
pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]
pci 0000:01:00.0: BAR 0: can't assign mem (size 0x1000000)
pci 0000:01:00.0: BAR 4: can't assign mem (size 0x10000)
pci 0000:01:00.0: BAR 5: can't assign mem (size 0x1000)
pci 0000:00:00.0: PCI bridge to [bus 01]
pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
pci 0000:01:00.0: Signaling PME through PCIe PME interrupt
pcie_pme 0000:00:00.0:pcie01: service driver pcie_pme loaded
Hi Yuri,
Here is the link for my discussion if you can help with:
Re: Adding PCI-e device driver for SABRE-SD board
Regards,
Phan. Douangphachanh