i.MX6ULL versions with lower count interfaces (ENET, UART, USB,...)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6ULL versions with lower count interfaces (ENET, UART, USB,...)

跳至解决方案
951 次查看
janezdolenc
Contributor I

Hello ,

I am starting HW design with i.MX6ULL. i.MX6ULL supports up to 2 Ethernet interfaces (ENET1 and ENET2), but I am using version with only 1 Ethernet (MCIMX6Y1CVM05AB ).

I couldn't find information in DS and RM which interface is active ENET1 or ENET2 ?

The same question could be for other interfaces (UART , I2C , USB , …).

It seems logical that first (or first 2 , or first 4) interface is active, it means ENET1 in my case, but I would like to get explicit information regarding this.

Regards ,

Janez Dolenc

标签 (1)
0 项奖励
回复
1 解答
946 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Janez

 

you are right, it is ENET1 and first active interfaces.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
947 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Janez

 

you are right, it is ENET1 and first active interfaces.

 

Best regards
igor

0 项奖励
回复