i.MX6ULL versions with lower count interfaces (ENET, UART, USB,...)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL versions with lower count interfaces (ENET, UART, USB,...)

ソリューションへジャンプ
953件の閲覧回数
janezdolenc
Contributor I

Hello ,

I am starting HW design with i.MX6ULL. i.MX6ULL supports up to 2 Ethernet interfaces (ENET1 and ENET2), but I am using version with only 1 Ethernet (MCIMX6Y1CVM05AB ).

I couldn't find information in DS and RM which interface is active ENET1 or ENET2 ?

The same question could be for other interfaces (UART , I2C , USB , …).

It seems logical that first (or first 2 , or first 4) interface is active, it means ENET1 in my case, but I would like to get explicit information regarding this.

Regards ,

Janez Dolenc

ラベル(1)
0 件の賞賛
返信
1 解決策
948件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Janez

 

you are right, it is ENET1 and first active interfaces.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
949件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Janez

 

you are right, it is ENET1 and first active interfaces.

 

Best regards
igor

0 件の賞賛
返信