i.MX6UL with Secure Boot and HAB errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL with Secure Boot and HAB errors

ソリューションへジャンプ
13,407件の閲覧回数
kinezo
Contributor III

I can't seem to find definitive information on what the cause may be to the HAB Event error of (0x22) or HAB_INV_ADDRESS.

--------- HAB Event 1 -----------------
event data:
   0xdb 0x00 0x08 0x42 0x33 0x22 0x0a 0x00

   STS = HAB_FAILURE (0x33)
   RSN = HAB_INV_ADDRESS (0x22)
   CTX = HAB_CTX_AUTHENTICATE (0x0A)
   ENG = HAB_ENG_ANY (0x00)

Can anyone help point me to the proper documentation?

I've gone through AN4581.pdf and HAB4_API.pdf and HABCST_UG.pdf.

Here's some further info about my setup.

Here's my CSF:

[Header]
Version = 4.2
Hash Algorithm = sha256
Engine = SW
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Unlock]
Engine = CAAM
Features = RNG

[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target Index = 2
# Key to install
File= "../crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem"

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Address Offset Length Data File Path
Blocks = 0x877ff400 0x0 0x074000 "./u-boot-padded.imx"

my u-boot.imx is 0x73c00 in size padded to 0x74000 using the documented objcopy command:

objcopy -I binary -O binary --pad-to 0x74000 --gap-fill=0x5A u-boot.imx u-boot-padded.imx

IVT looks like:

> xxd -g 4 -l 48 u-boot-signed.imx
0000000: d1002040 00008087 00000000 2cf47f87 .. @........,...
0000010: 20f47f87 00f47f87 00308787 00000000 ........0......
0000020: 00f07f87 00600700 00000000 d201e040 .....`.........@

Any help/pointers/tips to get me going in the right direction would be greatly appreciated. Thanks!

ラベル(1)
1 解決策
12,439件の閲覧回数
kinezo
Contributor III

Actually, now that I look back at the thread, I think I know why it didn't work. :smileyhappy:

Whatever instructions I read, had them padding the u-boot.imx. That doesn't make sense because the CSF goes at the end of it and the start address of the CSF is IN the IVT. If you pad u-boot, that'll push the CSF beyond where the IVT says it is!!

This time around, I didn't pad the u-boot blob. I'm not 100% certain, but i'm fairly confident that's why it didn't work the first time around.

Thanks again!

元の投稿で解決策を見る

22 返答(返信)
799件の閲覧回数
kinezo
Contributor III

Thanks Yuri, I'll check out that thread and see if that affects me. I realized, maybe I should attach the full HAB events, just in case:

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x08 0x42 0x33 0x22 0x0a 0x00

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ADDRESS (0x22)
CTX = HAB_CTX_AUTHENTICATE (0x0A)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x00
0x00 0x00 0x00 0x20

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x2c
0x00 0x00 0x01 0xe0

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x20
0x00 0x00 0x00 0x01

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 5 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x80 0x00 0x00
0x00 0x00 0x00 0x04

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)

Thanks!

0 件の賞賛
返信
799件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Appendix A (Interpreting HAB Event Data from Report_Event() API) of the “HAB4_API.pdf”

in the CST package should be used to analyze HAB Events.

  As for  reason  "HAB_INV_ADDRESS (0x22)  Invalid address: access denied",
please check if initialization via DCD table meet allowed addresses.
Please take a look at Table 8-31 (Valid DCD Address Ranges) in the i.MX 6UltraLite 

Reference Manual, Rev. 1, 04/2016.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信