i.MX6UL fuse prog for eMMC boot failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL fuse prog for eMMC boot failed

Jump to solution
2,590 Views
wandreas
Contributor II

Hi,

I tried to set the fuses of an i.MX6UL so, that it boots from eMMC.
Thus, I have worked out these bits for BOOT_CFG[1-4] according to the i.MX6UL Reference Manual:

01101101 11001000 (00000000) 00000000 = 0x6dc80000

I have burnt these bits in U-BOOT using the following line:

fuse prog 0 5 0x6dc80000

As far as I know, the processor also needs bank 0 word 6: BT_FUSE_SEL set to 1, to boot according to the fuse settings?

Thus I also performed:

fuse prog 0 6 0x00000010

The thing now is, that I broke the board. I cannot boot anymore.

I would like to know if I have done everything right, especially calculating the bits 0x6dc80000 and 0x00000010 ?

Thanks in Advance!


The BOOT_CFG bits I wanted to set are following (see UL Reference p. 208: Table 5-6. MMC/eMMC Boot Fusemap):

BOOT_CFG1[7,6,5] to select eMMC. 
BOOT_CFG1[3] to set normal mmc speed.

BOOT_CFG1[2] (Disable fast boot acknowledge, as we did not enable fast boot)
BOOT_CFG1[1]: 0 => no power cycle.

BOOT_CFG1[0]: 1: Loopback Clk Src: direct.

BOOT_CFG2[7,6,5]: 110  ... 8 bit DDR. 

BOOT_CFG2[4,3]:    01    ... eSDHC2

BOOT_CFG2[2]:       0      ... 400MHz

BOOT_CFG2[1]:       0      ... 3.3V SD Voltage.

Rest is 0. (CFG3 is reserved and CFG4 is all 0)

Labels (2)
Tags (1)
1 Solution
1,829 Views
Yuri
NXP Employee
NXP Employee

Hello,

BOOT_CFG1 - bits [7:0]
BOOT_CFG2 - bits [15:8]

BOOT_CFG3 - bits [23:16]

BOOT_CFG4 - bits [31:24]

 

 So, for 0x0000c86d -

BOOT_CFG1: 6d

BOOT_CFG2: c8

BOOT_CFG3: 00

BOOT_CFG4: 00

 

  This means Regular Boot , SD/MMC Speed Normal, Bus Width 8-bit (1-bit may

be used at first for test), eSDHC2.

Regards,

Yuri.

View solution in original post

2 Replies
1,830 Views
Yuri
NXP Employee
NXP Employee

Hello,

BOOT_CFG1 - bits [7:0]
BOOT_CFG2 - bits [15:8]

BOOT_CFG3 - bits [23:16]

BOOT_CFG4 - bits [31:24]

 

 So, for 0x0000c86d -

BOOT_CFG1: 6d

BOOT_CFG2: c8

BOOT_CFG3: 00

BOOT_CFG4: 00

 

  This means Regular Boot , SD/MMC Speed Normal, Bus Width 8-bit (1-bit may

be used at first for test), eSDHC2.

Regards,

Yuri.

1,829 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Hope the the following thread helps regarding BOOT_CFG.

eMMC Fuses And Card did not respond to voltage select! I.MX6UL 

  Also,  I can send You the mentioned there considerations via e-mail,

if You provide me Your e-mail.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply