Hi,
I tried to set the fuses of an i.MX6UL so, that it boots from eMMC.
Thus, I have worked out these bits for BOOT_CFG[1-4] according to the i.MX6UL Reference Manual:
01101101 11001000 (00000000) 00000000 = 0x6dc80000
I have burnt these bits in U-BOOT using the following line:
fuse prog 0 5 0x6dc80000
As far as I know, the processor also needs bank 0 word 6: BT_FUSE_SEL set to 1, to boot according to the fuse settings?
Thus I also performed:
fuse prog 0 6 0x00000010
The thing now is, that I broke the board. I cannot boot anymore.
I would like to know if I have done everything right, especially calculating the bits 0x6dc80000 and 0x00000010 ?
Thanks in Advance!
The BOOT_CFG bits I wanted to set are following (see UL Reference p. 208: Table 5-6. MMC/eMMC Boot Fusemap):
BOOT_CFG1[7,6,5] to select eMMC.
BOOT_CFG1[3] to set normal mmc speed.
BOOT_CFG1[2] (Disable fast boot acknowledge, as we did not enable fast boot)
BOOT_CFG1[1]: 0 => no power cycle.
BOOT_CFG1[0]: 1: Loopback Clk Src: direct.
BOOT_CFG2[7,6,5]: 110 ... 8 bit DDR.
BOOT_CFG2[4,3]: 01 ... eSDHC2
BOOT_CFG2[2]: 0 ... 400MHz
BOOT_CFG2[1]: 0 ... 3.3V SD Voltage.
Rest is 0. (CFG3 is reserved and CFG4 is all 0)
已解决! 转到解答。
Hello,
BOOT_CFG1 - bits [7:0]
BOOT_CFG2 - bits [15:8]
BOOT_CFG3 - bits [23:16]
BOOT_CFG4 - bits [31:24]
So, for 0x0000c86d -
BOOT_CFG1: 6d
BOOT_CFG2: c8
BOOT_CFG3: 00
BOOT_CFG4: 00
This means Regular Boot , SD/MMC Speed Normal, Bus Width 8-bit (1-bit may
be used at first for test), eSDHC2.
Regards,
Yuri.
Hello,
BOOT_CFG1 - bits [7:0]
BOOT_CFG2 - bits [15:8]
BOOT_CFG3 - bits [23:16]
BOOT_CFG4 - bits [31:24]
So, for 0x0000c86d -
BOOT_CFG1: 6d
BOOT_CFG2: c8
BOOT_CFG3: 00
BOOT_CFG4: 00
This means Regular Boot , SD/MMC Speed Normal, Bus Width 8-bit (1-bit may
be used at first for test), eSDHC2.
Regards,
Yuri.
Hello,
Hope the the following thread helps regarding BOOT_CFG.
eMMC Fuses And Card did not respond to voltage select! I.MX6UL
Also, I can send You the mentioned there considerations via e-mail,
if You provide me Your e-mail.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------