i.MX6UL fast-path function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL fast-path function

2,111 Views
tangwang
Contributor I

Whether i.MX6UL can handle LAN/WAN configuration(via VLAN config) or not ? like what Ethernet switch did(routing package from LAN to WAN without consume CPU computing power) ? if no, what is the computing power need if we want to implement it(routing feature) by NXP CPU ? will this increase package latency ?

Labels (1)
0 Kudos
Reply
2 Replies

1,991 Views
tangwang
Contributor I

Hi Sir,

Do you have any example or source code for our reference?

0 Kudos
Reply

1,991 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tang

I am afraid there is no hardware support for such capability and

cpu usage is needed.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply