i.MX6UL codec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL codec

Jump to solution
3,577 Views
JHY
Contributor IV

According to the datasheet, I.MX6UL has no HW video codec.

Maybe it can use SW codec for encoding MJPEG or H264.

I want to know SW codec capability of IMX6UL under Android OS.

Are there documents about performance test or resource usages?

Labels (1)
0 Kudos
Reply
1 Solution
3,005 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

as android is based on linux one can use attached Release Notes info in

Table 23. Video codec specification for hardware without VPU acceleration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,006 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

as android is based on linux one can use attached Release Notes info in

Table 23. Video codec specification for hardware without VPU acceleration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply