i.MX6UL codec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,575件の閲覧回数
JHY
Contributor IV

According to the datasheet, I.MX6UL has no HW video codec.

Maybe it can use SW codec for encoding MJPEG or H264.

I want to know SW codec capability of IMX6UL under Android OS.

Are there documents about performance test or resource usages?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,003件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

as android is based on linux one can use attached Release Notes info in

Table 23. Video codec specification for hardware without VPU acceleration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,004件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

as android is based on linux one can use attached Release Notes info in

Table 23. Video codec specification for hardware without VPU acceleration

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信