i.MX6UL Security Features

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL Security Features

1,535件の閲覧回数
dsnknd
Contributor I

Hi,

According to i.MX6 UltraLite ordering information, some parts offer Standard Security, Enhanced Security or both.

From the "i.MX6 and i.MX 7 Series Comparison Table" Security Features (https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf) , which features below are "Standard" and which are "Enhanced"?

1. Secure Boot

2. RNG

3. Tamper Detection

4. Secure Storage (including 32 KB Secure RAM)

5. Cryptographic Accelerators (AES-128, DES 3DES, ARC4, MD5, SHA-1, SHA-224, SHA-256, RSA/ECDSA)

6. Secure Debug,

7. OTP Space

Best Regards.

ラベル(1)
0 件の賞賛
返信
1 返信

1,457件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the following helps:

https://community.nxp.com/message/1181388 

Regards,

Yuri.

0 件の賞賛
返信