i.MX6UL Security Features

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL Security Features

1,512 Views
dsnknd
Contributor I

Hi,

According to i.MX6 UltraLite ordering information, some parts offer Standard Security, Enhanced Security or both.

From the "i.MX6 and i.MX 7 Series Comparison Table" Security Features (https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf) , which features below are "Standard" and which are "Enhanced"?

1. Secure Boot

2. RNG

3. Tamper Detection

4. Secure Storage (including 32 KB Secure RAM)

5. Cryptographic Accelerators (AES-128, DES 3DES, ARC4, MD5, SHA-1, SHA-224, SHA-256, RSA/ECDSA)

6. Secure Debug,

7. OTP Space

Best Regards.

Labels (1)
0 Kudos
Reply
1 Reply

1,434 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the following helps:

https://community.nxp.com/message/1181388 

Regards,

Yuri.

0 Kudos
Reply