i.MX6UL PXP really supports EPD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL PXP really supports EPD?

ソリューションへジャンプ
1,909件の閲覧回数
torus1000
Contributor V

Hi all,

I believe i.MX6UL PXP supported EPD/e-ink but I could find just 1 line in reference manual as following.

      p2421 and 2423
      This is used for 16bpp gamma correction or EPD color panel support.

Does i.MX6UL PXP really support EPD? Is there any documents which described the usage of EPD?

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,551件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

IMX6UL does not support EPD ; it has no EPDC.
The PXP module as coprocessor can work with different data.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,552件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

IMX6UL does not support EPD ; it has no EPDC.
The PXP module as coprocessor can work with different data.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信