i.MX6UL PXP really supports EPD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL PXP really supports EPD?

Jump to solution
895 Views
torus1000
Contributor V

Hi all,

I believe i.MX6UL PXP supported EPD/e-ink but I could find just 1 line in reference manual as following.

      p2421 and 2423
      This is used for 16bpp gamma correction or EPD color panel support.

Does i.MX6UL PXP really support EPD? Is there any documents which described the usage of EPD?

Thanks

Labels (1)
Tags (1)
0 Kudos
1 Solution
537 Views
Yuri
NXP Employee
NXP Employee

Hello,

IMX6UL does not support EPD ; it has no EPDC.
The PXP module as coprocessor can work with different data.


Have a great day,
Yuri
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
538 Views
Yuri
NXP Employee
NXP Employee

Hello,

IMX6UL does not support EPD ; it has no EPDC.
The PXP module as coprocessor can work with different data.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos