i.MX6UL Linux ECSPI2_MISO on UART5_RX pin misconfiguration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL Linux ECSPI2_MISO on UART5_RX pin misconfiguration

1,320件の閲覧回数
compmas2
Contributor V


The input select configuration for the ECSPI2_MISO functionality being assigned to the UART5_RX_DATA pin is incorrectly configured for the i.MX6UL in the imx_3.14.52_1.1.0_ga and imx_3.14.38_6ul_ga kernels.  Specifically the Daisy Chain input register address and value is not present. Attached is a patch to the issue which was verified working on a custom i.MX6UL board.

Original Attachment has been moved to: imx6ul_3.14.52_1.1.0_ga_ecspi2_miso_to_uart5_rx_input_select_fix.patch.zip

ラベル(3)
0 件の賞賛
返信
1 返信

1,195件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   I forwarded this the the team.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信