i.MX6UL Linux ECSPI2_MISO on UART5_RX pin misconfiguration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL Linux ECSPI2_MISO on UART5_RX pin misconfiguration

1,316 次查看
compmas2
Contributor V


The input select configuration for the ECSPI2_MISO functionality being assigned to the UART5_RX_DATA pin is incorrectly configured for the i.MX6UL in the imx_3.14.52_1.1.0_ga and imx_3.14.38_6ul_ga kernels.  Specifically the Daisy Chain input register address and value is not present. Attached is a patch to the issue which was verified working on a custom i.MX6UL board.

Original Attachment has been moved to: imx6ul_3.14.52_1.1.0_ga_ecspi2_miso_to_uart5_rx_input_select_fix.patch.zip

标签 (3)
0 项奖励
回复
1 回复

1,191 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   I forwarded this the the team.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复