i.MX6UL ADC: VrefH input current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6UL ADC: VrefH input current

ソリューションへジャンプ
1,532件の閲覧回数
johannesdev
Contributor III

Hi!

We are designing an application with the i.MX6UL's internal ADC in use. An external shut voltage reference is connected to the SoC's VrefH input.

However, the datasheet of the i.MX6UL does not specify the input current on pin VrefH. Thus, I cannot calculate an appropriate bias current for the shunt reference. Is this value known?

Best regards,
Johannes

0 件の賞賛
返信
1 解決策
1,475件の閲覧回数
art
NXP Employee
NXP Employee

The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.

Best Regards,
Artur

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,476件の閲覧回数
art
NXP Employee
NXP Employee

The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.

Best Regards,
Artur

0 件の賞賛
返信