i.MX6UL ADC: VrefH input current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL ADC: VrefH input current

Jump to solution
1,523 Views
johannesdev
Contributor III

Hi!

We are designing an application with the i.MX6UL's internal ADC in use. An external shut voltage reference is connected to the SoC's VrefH input.

However, the datasheet of the i.MX6UL does not specify the input current on pin VrefH. Thus, I cannot calculate an appropriate bias current for the shunt reference. Is this value known?

Best regards,
Johannes

0 Kudos
Reply
1 Solution
1,466 Views
art
NXP Employee
NXP Employee

The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.

Best Regards,
Artur

View solution in original post

0 Kudos
Reply
1 Reply
1,467 Views
art
NXP Employee
NXP Employee

The ADC_VREFH pin behaves as a regular FET gate input, so, its leakage current is negligible.

Best Regards,
Artur

0 Kudos
Reply