Hi,
We have new i.MX6SX based custom HW. Everything else seems to be working ok, but I'm having hard time getting Ethernet working.
I'm running Linux 4.1.38 built using Yocto 2.2. We have LAN8720 PHY - chip. Linux is able to see the eth0 device and when the Ethernet link is up/down, but no data comes/goes ie. if I set static IP ping doesn't go through either way.
Here is the device tree how I configure here the pins and device
pinctrl_enet1: enet1grp {
fsl,pins = <
MX6SX_PAD_ENET1_MDC__ENET1_MDC 0x1b0d9
MX6SX_PAD_ENET1_MDIO__ENET1_MDIO 0x1b0d9
MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x1b0d9
MX6SX_PAD_RGMII1_RD0__ENET1_RX_DATA_0 0x1b0d9
MX6SX_PAD_RGMII1_RD1__ENET1_RX_DATA_1 0x1b0d9
MX6SX_PAD_RGMII1_RXC__ENET1_RX_ER 0x1b0d9
MX6SX_PAD_RGMII1_RX_CTL__ENET1_RX_EN 0x1b0d9
MX6SX_PAD_RGMII1_TD0__ENET1_TX_DATA_0 0x1b0d9
MX6SX_PAD_RGMII1_TD1__ENET1_TX_DATA_1 0x1b0d9
MX6SX_PAD_RGMII1_TX_CTL__ENET1_TX_EN 0x1b0d9
>;
};
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;
phy-mode = "rgmii";
phy-id = <0>;
status = "okay";
};
HW guy has measured the signals and said that they looked good so I'm assuming that pin config is 'close enough' for it to work.
I'm running out of ideas what could be wrong. Do I need to config driver/phy now differently since we only are using half the data lines in RGMII - bus? Wasn't able to find info about that.
已解决! 转到解答。
I got this working. The problem was in the RGMII/RMII bus - configuration.
I changed this line
phy-mode = "rgmii";
to this
phy-mode = "rmii";
And network started working! Didn't catch that before.
An ethernet system consists of the MAC block (inside i.MX) and the PHY (outside). Both of them must have a clock source for correct operation. I'm rather sure that you checked that there is a clock, but you can only measure this at the outside. You can't check if the internal block has a clock source. You can only make sure that there is an internal clock by programming it correctly :-)
Example:
Hoping that this was the root cause for your problem.
I got this working. The problem was in the RGMII/RMII bus - configuration.
I changed this line
phy-mode = "rgmii";
to this
phy-mode = "rmii";
And network started working! Didn't catch that before.