Silex SDCAN2 WiFi AP mode not working with iMX6ULL EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Silex SDCAN2 WiFi AP mode not working with iMX6ULL EVK

654 Views
whizpb
Contributor I

I am using a Silex SDCAN2 module with MCIMX6ULL EVK. The SDCAN2 module works well in Wi-Fi Client mode however fails to work in AP mode. Hostapd is used for enabling AP mode. The AP mode comes up for a short interval and then dies out with no failure prints coming up on hostapd. The interface is also up and available on the host. 

Following are the components and configuration used.
BSP: fsl-yocto-L4.1.15_2.1.0-ga.tar.gz
Hostapd Config:
interface=wlan0
ctrl_interface=/var/run/hostapd
bridge=br0
driver=nl80211
ssid=ath6ap
channel=6
wpa=0
eap_server=1
wps_state=0
beacon_int=100
hw_mode=g
max_num_sta=8
wme_enabled=1
Any leads to resolve this are appreciated.
Labels (2)
0 Kudos
1 Reply

501 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prashant

silex modules are not supported in nxp official bsps starting from L3.14.52.

One can try to port older releases found on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

or apply to silex support (Contact Silex Support ) for updated driver or look at third party releases

New Silex WiFi 802.11ac and BT4.1 module - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos