i.MX6SDL GC880 performance.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6SDL GC880 performance.

ソリューションへジャンプ
5,121件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL GPU performance.

I want to know the performance of GC880 in i.MX6SDL, but I did not find the following performances.

Pixel Rate (MPixel/sec)

Triangle Rate (M tri/sec)

Vertext Rate (M vtx/sec)

Shader GFLOPS

So would you let me kwno the performances?

Best Regards,

Satoshi Shimoda

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
3,564件の閲覧回数
art
NXP Employee
NXP Employee

The available performance data for the Vivante GC880 3D graphics core are as follows.

Pixel rate is 266Mpix/s.

Triangle rate is 35Mtri/s.

Vertex rate is about 100Mvtx/s.

Shader GFLOPS rate is 3.2.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,565件の閲覧回数
art
NXP Employee
NXP Employee

The available performance data for the Vivante GC880 3D graphics core are as follows.

Pixel rate is 266Mpix/s.

Triangle rate is 35Mtri/s.

Vertex rate is about 100Mvtx/s.

Shader GFLOPS rate is 3.2.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信