i.MX6Quad Jumpstart Development Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Quad Jumpstart Development Kit

1,070 Views
vittoria98
Contributor I

Good morning everyone, 

I have the Connectcore 6 for i.MX6Quad Jumpstart development kit, and I'm trying to test its JTAG connections. 

I've uploaded the netlist, BOM, schematic, and BSDL file. The board is connected to JTAG link2 through  Tag-Connect’s TC2050-IDC-NL “No Legs” Plug-of-Nails™ cable and an ARM 20-pin to ARM 10-pin. 

This is the error I get: 

Starting Check Chain...

 

No valid data returned from the JTAG chain.
Perhaps the pin map is incorrect, or the board is not powered.

 

Check Chain failed

I believe there is a problem with the pin mapping/reset sequence, but I can't figure out what it is; can you help me with that? 

Thank you, 

Vittoria

 

0 Kudos
Reply
1 Reply

1,057 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @vittoria98 ,

I hope you are doing well.

Could you please check with the other JTAG device?

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply