i.MX6Q-error display on LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q-error display on LCD

ソリューションへジャンプ
2,153件の閲覧回数
全运曾
Contributor I

Hi,

I have built a Linux 3.0.35 kernel for a LCD. At the beginning, there was a correct display on the LCD. However, after setting up an SD/MMC card by using MFGTool or Linux Host for several times, the display on the LCD is wrong, while using the same u-boot, uImage and file system. The final image on the LCD is the image with four penguins on the top left corner.


Here is the bottom of the terminal output.

starting pid 1392, tty '': '/etc/rc.d/rcS'

Mounting /proc and /sys

Starting the hotplug events dispatcher udevd

udevd (1401): /proc/1401/oom_adj is deprecated, please use /proc/1401/oom_score_

adj instead.

Synthesizing initial hotplug events

Setting the hostname to freescale

Mounting filesystems

BusyBox v1.20.2 () multi-call binary.

Usage: mount [OPTIONS] [-o OPTS] DEVICE NODE

Mount a filesystem. Filesystem autodetection requires /proc.

        -a              Mount all filesystems in fstab

        -r              Read-only mount

        -w              Read-write mount (default)

        -t FSTYPE[,...] Filesystem type(s)

        -O OPT          Mount only filesystems with option OPT (-a only)

-o OPT:

        loop            Ignored (loop devices are autodetected)

        [a]sync         Writes are [a]synchronous

        [no]atime       Disable/enable updates to inode access times

        [no]diratime    Disable/enable atime updates to directories

        [no]relatime    Disable/enable atime updates relative to modification ti

me

        [no]dev         (Dis)allow use of special device files

        [no]exec        (Dis)allow use of executable files

        [no]suid        (Dis)allow set-user-id-root programs

        [r]shared       Convert [recursively] to a shared subtree

        [r]slave        Convert [recursively] to a slave subtree

        [r]private      Convert [recursively] to a private subtree

        [un]bindable    Make mount point [un]able to be bind mounted

        [r]bind         Bind a file or directory [recursively] to another locati

on

        move            Relocate an existing mount point

        remount         Remount a mounted filesystem, changing flags

        ro/rw           Same as -r/-w

There are filesystem-specific -o flags.

mount: mounting usbfs on /proc/bus/usb failed: No such file or directory

starting pid 3128, tty '': '/etc/rc.d/rc_gpu.S'

/etc/rc.d/rc_gpu.S: line 6: /sys/module/galcore/parameters/gpu3DMinClock: No suc

h file or directory

starting pid 3134, tty '': '/etc/rc.d/rc_mxc.S'

arm-none-linux-gnueabi-gcc (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/

10 09:20) 4.6.2 20110630 (prerelease)

root filesystem built on Fri, 28 Feb 2014 20:05:30 +0800

Freescale Semiconductor, Inc.

freescale login:

Can anybody help me to get an correct display on LCD?

ラベル(3)
1 解決策
1,858件の閲覧回数
全运曾
Contributor I

Thanks for the information. The uboot, uImage and file system have been downloaded successfully. And the setting of uboot environment is right.

Finally, it is ok when I download file system from rootfs.ext2 in the L3.0.35_4.1.0_130816_images_MX6 instead of from the rootfs folder in ltib folder.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,858件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Zeng,

Have you download the uboot, uImage and file system to your board succeed ? And if the setting of uboot environment is right. Would you please check?

Have a great day

Best Regards
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,859件の閲覧回数
全运曾
Contributor I

Thanks for the information. The uboot, uImage and file system have been downloaded successfully. And the setting of uboot environment is right.

Finally, it is ok when I download file system from rootfs.ext2 in the L3.0.35_4.1.0_130816_images_MX6 instead of from the rootfs folder in ltib folder.

0 件の賞賛
返信
1,858件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi zeng,

I recommend you to create the thread in right place i.MX Community, so you can get quick response.

Best Regards

Dan

0 件の賞賛
返信