i.MX6Q RWS_EN for Bayer/Raw image capture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q RWS_EN for Bayer/Raw image capture

Jump to solution
2,414 Views
davemcmordie
Contributor III

Section 37.5.142 of the Reference Manual (IPUx_IC_CONF) refers to RWS_EN (Raw Sensor Enable).  It looks like this and CSI_MEM_WR_EN need to be set correctly to enable raw/Bayer/Monochrome sensors.  Yet I don't see this setting being set in the CSI_MEM case in the enable tasks method of ipu_ic.  Is this setting necessary to enable raw image capture, or is there another way to do it?

Labels (3)
0 Kudos
Reply
1 Solution
1,983 Views
jamesbone
NXP TechSupport
NXP TechSupport

Yes, it is just another way to do it,  the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP  the general way to do it, but can be done just like you mention

View solution in original post

0 Kudos
Reply
1 Reply
1,984 Views
jamesbone
NXP TechSupport
NXP TechSupport

Yes, it is just another way to do it,  the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP  the general way to do it, but can be done just like you mention

0 Kudos
Reply