i.MX6Q RWS_EN for Bayer/Raw image capture

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6Q RWS_EN for Bayer/Raw image capture

跳至解决方案
2,425 次查看
davemcmordie
Contributor III

Section 37.5.142 of the Reference Manual (IPUx_IC_CONF) refers to RWS_EN (Raw Sensor Enable).  It looks like this and CSI_MEM_WR_EN need to be set correctly to enable raw/Bayer/Monochrome sensors.  Yet I don't see this setting being set in the CSI_MEM case in the enable tasks method of ipu_ic.  Is this setting necessary to enable raw image capture, or is there another way to do it?

标签 (3)
0 项奖励
回复
1 解答
1,994 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Yes, it is just another way to do it,  the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP  the general way to do it, but can be done just like you mention

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,995 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Yes, it is just another way to do it,  the IPU it is very flexible and allows different ways to get the same task. So the we use in the BSP  the general way to do it, but can be done just like you mention

0 项奖励
回复