i.MX6Q LVDS split mode outputs LVDS1 only

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q LVDS split mode outputs LVDS1 only

Jump to solution
10,902 Views
torus1000
Contributor V

Hi,

I have 1920x1080 LVDS panel and modified device tree source (dtsi) of i.mx6q yocto L.3.10.53.
Then I tried ldb split mode (ldb=spl0) as following.

  U-Boot> setenv displayinfo video=mxcfb1:dev=ldb,if=RGB24 ldb=spl0 fbmem=24M
  ...
  U-Boot> boot
  ...

  Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw
  video=mxcfb1:dev=ldb,if=RGB24 ldb=spl0 fbmem=24M
  ...


LVDS1 looked OK but LVDS0 (neither clock nor data) output nothing.

Can anyone help me to output both LVDS ports in split mode(2 ports for 1 panel)?

Actual fbset was as following...

  > fbset
  mode "960x1080-52"
      # D: 74.250 MHz, H: 60.861 kHz, V: 52.018 Hz
      geometry 960 1080 960 1088 16
      timings 13468 60 60 23 22 140 45
      rgba 5/11,6/5,5/0,0/0
  endmode

Thanks.

Labels (4)
1 Solution
5,318 Views
torus1000
Contributor V

Dear Saurabh and Guanqiong,

Freescale local FAE kindly sent us a patch as following.
After applying this patch, it worked.
It seems additional "split-mode;" line required to resolve my issue.

Hava a nice day!

//patch//
--- a/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
+++ b/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
@@ -505,46 +505,47 @@

&ldb {
  status = "okay";
+ split-mode;

  lvds-channel@0 {
   fsl,data-mapping = "spwg";
...

View solution in original post

5 Replies
5,318 Views
joanxie
NXP TechSupport
NXP TechSupport

did you add your lvds to the ldb.c? pls refer to the link as below:

Re: i.MX6 Dual LVDS Support

0 Kudos
Reply
5,319 Views
torus1000
Contributor V

Dear Saurabh and Guanqiong,

Freescale local FAE kindly sent us a patch as following.
After applying this patch, it worked.
It seems additional "split-mode;" line required to resolve my issue.

Hava a nice day!

//patch//
--- a/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
+++ b/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
@@ -505,46 +505,47 @@

&ldb {
  status = "okay";
+ split-mode;

  lvds-channel@0 {
   fsl,data-mapping = "spwg";
...

5,318 Views
osmarfrisonjun1
Contributor III

Hello,

How do I do to apply this changes to a new .sdcard?

Thanks.

0 Kudos
Reply
5,318 Views
saurabh206
Senior Contributor III

Hi Torus

Thanks for posting the solution.

Saurabh

5,318 Views
saurabh206
Senior Contributor III

Hi

Torus

You need to add display information to struct fb_videomode ldb_modedb according to your resolution.

Can you try to verify ldb driver and dtb file initialization?

Why you have selected video=mxcfb1 ? You can use video=mxcfb0 with dtb setting.

Thanks

Saurabh

0 Kudos
Reply